Measurement Setup Parameters (Keysight X-Series Analyzers)
This topic provides measurement configuration and setup parameter information that apply to using the Keysight X-Series Signal Analyzer hardware with the 89600 VSA software. This information will help to properly setup the 89600 VSA and Keysight X-Series Signal Analyzer measurement parameters.
Auto-range Criteria
![]()
The availability of Auto-Range Criteria choices (located on the VSA's main toolbar) depends on the connected hardware model and IF path. See Auto-Range Criteria for more information.
This choice is supported for all models and IF Paths.
This choice is supported for all models and IF Paths.
This choice is supported with the following models and IF paths:
- Models: N9020, N9021, N9030, N9032, N9040, N9041, N9042
- IF Paths: 25 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second. (Opt B25)*, 140 MHz (Opt B1X), 160 MHz (Opt B1Y), 255 MHz (Opt B2X), 510 MHz (Opt B5X), 1 GHz Gigahertz: A frequency measurement which equals one billion hertz. (Opt H1G or Opt R10), 1.5 GHz (Opt R15), 2 GHz (Opt R20)
* Not supported with N9032.
Calibration/Alignment
Selecting Calibrate () will initiate a full calibration and alignment.
Selecting Quick Cal () will initiate a smart calibration procedure. The Quick Cal only performs an alignment procedure on sections of the hardware that need re-alignment. Quick Cal is faster than the Calibrate procedure and when completed, the entire instrument is aligned and calibrated. When the Auto Calibrate check box is selected, a Quick Cal is performed whenever the VSA determines the hardware needs to be re-calibrated.
When Auto Calibrate is selected (), the VSA monitors the calibration status and automatically performs a Quick Cal when required.
Custom Channel Configurations
The Custom Channel Configurations dialog ) is used to create custom channel mapping configurations, that is, you can reconfigure the hardware input channel to VSA measurement channel connections. The VSA only allows valid channel configuration mappings; "invalid" channel configuration mappings are disallowed (indicated by a red "X") and the "OK" button is disabled "greyed out".
Different X-Series analyzer models and options support different input channel configurations and available measurement types. The following tables can be used to determine what models and options support single and dual instrument configurations and what measurement types are supported.
Supported X-Series Instrument Configurations
Many X-Series instrument models can be used in single and dual instrument hardware configurations. The following table lists the X-series models and options that support single and dual instrument hardware configurations:
X-Series
Instrument
Single
Instrument ConfigurationsDual
Instrument Configurations1UXA (except N9042B) YES NO UXA (N9042B) YES YES PXA YES NO MXA YES YES2 except NO when options DP2 & B40 are installed.
EXA YES YES2 except NO when options DP2 & B40 are installed.
MXE YES NO PXE YES NO CXA YES NO CXA-m YES NO notes: 1) phase coherence is not supported.
2) only MXA/EXA signal analyzers with "A" model numbers support dual instrument configurations.
Supported Input Channel Measurement Types
Input Channel Type Single Instrument Configuration
(Measurement Type)
Dual Instrument Configuration
(Measurement Type)
RF Radio Frequency: A generic term for radio-based technologies, operating between the Low Frequency range (30k Hz) and the Extra High Frequency range (300 GHz).: 1 Channel RF measurement
1 and 2 Channel RF measurements1
Baseband: 1 Channel baseband (I input only) measurement2
2 Channel baseband (I & Q inputs only) measurement2
1 Channel baseband (I input only) measurement2
2 Channel baseband (I & Q inputs only) measurement2
I+jQ: single I+jQ channel measurement2,3,4
single I+jQ channel measurement2,3,4
External Mixer: 1 Channel measurement2
1 Channel measurement2
notes: 1) two Ch RF measurements require 2 analyzers.
2) all Baseband BBIQ (I, Q, & I+jQ) measurements require option BBA Analog Baseband I/Q Inputs installed.
3) dual I+jQ channel measurements are not supported.
4) for BBIQ (I+jQ) measurements using X-Series signal analyzers, the VSA's setting is always selected and disabled.
Custom Input Channel Configurations:When using the Input Channel Configuration dialog to specify or modify the input channel configuration mapping, only the VSA default set of channel configuration mappings are allowed; "invalid" channel configuration mappings are disallowed and the "" button is disabled "greyed out".
External Reference
The VSA automatically determines whether to use the internal or external frequency reference. The VSA will automatically switch to external frequency reference whenever a valid external reference signal is detected on the Ext Ref In port. When an invalid signal is detected (i.e., the signal frequency is incorrect) the VSA will indicate UNLOCKED.
Frequency Bands
The 89600 VSA supports the RF frequency band of the X-Series instrument and optional Baseband for instruments with option BBA installed.
Mixer Level
The 89600 VSA Mixer Level control adjusts the Input Attenuation and ADC Analog-to-Digital Converter Range of the VSA. The default Mixer Level setting set by the 89600 VSA software is represented as 0 dB. Any Mixer Level setting selected is relative to the default Mixer Level setting. The Mixer Level control is not applicable for baseband hardware option BBA. For more information on Mixer Level control, see Mixer Level.
Periodic Trigger
Periodic triggering specifies that triggering will occur at regularly spaced intervals.
Periodic Trigger is not supported for the following X-Series Signal Analyzer models/configurations:
- Aux Wideband path when using N9040B-H1G.
- N9041B Option EDC Configuration
When Periodic Trigger is selected (Acquisition > Trigger > Trigger tab), the following parameters are also available:
Delay: In periodic trigger mode, the value entered specifies an amount of delay from the periodic triggering point to the beginning of the acquisition data.
Period: Specifies the trigger interval.
Period Offset: Adds an offset relative to the periodic triggering point.
Sync Source: Selects a sync trigger source.
Preset Setup Parameters
The following table lists the Keysight X-Series Signal Analyzer's unique preset setup parameters and their default values. This table includes the parameters for the dual-channel baseband option, BBA.To preset the VSA, select . (Any parameters not listed here are set to the standard Preset Setup values.)
|
Parameter |
Default setting (UXA/PXA/MXA/MXE/PXE) |
Default setting (EXA/CXA/CXA-m) |
Default Setting (I+jQ) |
|---|---|---|---|
|
Range |
20 dBm (default) 22 dBm (opt FSA) |
10 dBm | |
|
Center |
1 GHz |
1 GHz |
0 Hz |
|
Span |
10 MHz (default) 25 MHz (Opt B25) 40 MHz (Opt B40) 10 MHz (Opt B1X) 160 MHz (Opt B1Y) 255 MHz (Opt B2X) 510 MHz (Opt B5X) 1 GHz (Opt H1G or R10) 1.5 GHz (Opt R15) 2 GHz (Opt R20) 4 GHz (Opt R40) |
10 MHz 25 MHz (Opt B25) 40 MHz (Opt B40) |
Max licensed span |
|
ResBW |
100 kHz kiloHertz: A radio frequency measurement (one kilohertz = one thousand cycles per second). (default) 300 kHz (Opt B25) 300 KHz (Opt B40) 1 MHZ (Opt B1X) 1 MHZ (Opt B1Y) 3 MHZ (Opt B2X) 3 MHZ (Opt B5X) 10 MHz (Opt H1G or R10) 10 MHz (Opt R15) 10 MHz (Opt R20) 30 MHz (Opt R40) |
100 kHz 300 kHz (Opt B25) 300 kHz (Opt B40) |
300 kHz |
|
Time Parameters: |
|
|
|
|
Main Time Length |
38.20 µs (default) 12.25 µs (Opt B25) 12.73 µs (Opt B40) 3.82 µs (Opt B1X) 3.82 us (Opt B1Y) 1.27 us (Opt B2X) 1.27 us (Opt B5X) 382 ns (Opt H1G or R10) 382 ns (Opt R15) 382 ns (Opt R20) 127 ns (Opt R40) |
38.20 µs 12.25 us (Opt B25) 12.73 us (Opt B40) |
3.83 µs or licensed value |
|
Max Overlap |
90 % |
90 % |
90% |
|
Gate on/off |
Off |
Off |
Off |
|
Length |
1.4 µs |
1.4 µs |
1.4 µs |
The VSA always tries to capture data at a sample rate of 1.28x the span (2.56x the span for baseband time data). If the measurement hardware does not support this sample rate (typically near full span), the VSA will resample the data to 1.28x the span after receiving it from the measurement hardware so that it will be compatible with the VSA’s algorithms. See the Theory of Operation topic for more information.
Range
Input range can be selected by choosing a Full Scale Range in the 89600 VSA. After specifying the range, the VSA sets the optimal attenuator, ADC gain, and optional preamp on/off setting for the VSA to optimize dynamic range primarily for noise and secondarily for intermodulation distortion.
Input Overload Condition
For 2-Ch Baseband measurement configurations, out-of-band input signals will cause an unexpected ADC Overload condition, ("OV" trace indicator) when the following conditions occur:
- The Out-of-Band signal frequency "fo" is greater than the current VSA measurement bandwidth (20 MHz maximum) but less than the maximum hardware analog input channel bandwidth (40 MHz). Therefore: VSA BW < fo < 40 Mhz.
- Out-of-Band signals are combined with the VSA Measurement In-Band signals to determine the range level. An unexpected range overload will occur when the additional Out-of-Band signals cause the combined VSA measurement range level to exceed the current VSA measurement setting.
This Range Overload condition may seem unexpected because the Out-of-Band signals are not shown on the VSA Trace window hiding the over range signals from view.
Analyzer Min/Max Input Range UXA (N9042B)
-22 dBm to +30 dBm, non-preamp in 2 dB steps,
-40 dBm to -20 dBm, Low Noise Amplifier in 2 dB steps
w/Option 567 or 575 >= 50 GHz, -32 dBm to +16 dBm in 2 dB steps
UXA
-22 dBm to +30 dBm, non-preamp in 2 dB steps,
-42 dBm to +30 dBm, preamp f < 3.6 GHz in 2 dB steps
-56 dBm to +30 dBm, preamp f > 3.6 GHz in 2 dB steps
PXA (N9032B)
-22 dBm to +30 dBm, non-preamp in 2 dB steps,
-40 dBm to -20 dBm, Low Noise Amplifier in 2 dB steps
PXA
-22 dBm to +30 dBm, non-preamp in 2 dB steps,
-42 dBm to +30 dBm, preamp f < 3.6 GHz in 2 dB steps
-56 dBm to +30 dBm, preamp f > 3.6 GHz in 2 dB steps
MXA -20 dBm to +30 dBm, non-preamp in 2 dB steps,
-40 dBm to +30 dBm, preamp f < 3.6 GHz in 2 dB steps,
-56 dBm to +30 dBm, preamp f > 3.6 GHz in 2 dB steps
MXE -20 dBm to +30 dBm, non-preamp in 2 dB steps,
-40 dBm to +30 dBm, preamp f < 3.6 GHz in 2 dB steps,
-54 dBm to +30 dBm, preamp f > 3.6 GHz in 2 dB steps
PXE -22 dBm to +30 dBm, non-preamp in 2 dB steps,
-40 dBm to +30 dBm, preamp in 2 dB steps,
EXA -20 dBm to +20 dBm in 10 dB or opt 2 dB steps,
-20 dBm to +22 dBm w/Opt FSA in 10 dB or opt 2 dB steps,
-40 dBm to +20 dBm, preamp f < 3.6 GHz in 10 dB or opt 2 dB steps,
-56 dBm to +20 dBm, preamp f > 3.6 GHz in 10 dB or opt 2 dB steps
CXA -20 dBm to +20 dBm in 10 dB or opt 2 dB steps,
-20 dBm to +22 dBm w/Opt FSA in 10 dB or opt 2 dB steps,
-40 dBm to + 20 dBm, preamp in 10 dB or opt 2 dB steps,
CXA-m -40dBm to -20dBm in 10dB steps (f < 7.58GHz)
-20dBm to +20dBm in 10dB or opt 2dB steps w/Opt FSA (f < 7.58GHz)
-40dBm to +20dBm in 10dB in 10dB steps (f > 7.58GHz)
non-preamp f < 7.58 GHz in 2 dB steps,
non-preamp f > 7.58 GHz in 10 dB steps,
preamp in 10 dB steps
The minimum practical input range setting is -54 dB since the minimum supported attenuator step size is 2 dB and the step size is referenced from 0 dB.
The input range choices are limited by the mechanical attenuator step size of the instrument. The standard EXA/CXA/CXA-m step size is 10 dB, with an option for a 2 dB step size. The standard UXA/PXA/MXA/MXE/PXE step size is 2 dB.
Recording
The 89600 VSA records time data from the X-series analyzer hardware to the system hard drive. For most recording purposes, the length of time waveform recording is limited to the capture size. For actual capture size limits, see the analyzer hardware spec sheet.
Saving and Recalling VSA Setups
The VSA's state is not automatically saved when the 89600 VSA is closed; select before closing the application. When a saved setup is recalled into the 89600 VSA , the VSA state is restored from the setup.
Segmented Capture
Segmented capture is possible when the hardware has the following:
- All X-Series analyzers (except N9032B or N9042B):
- Hardware instrument software version A.21.10 or later
- Option DP4
- A wideband Digital IF (DIF) signal path that supports segmented capture (and has the right option to enable it). Currently supported analysis signal paths for segmented capture are:
- 255 MHz Analysis Bandwidth
- 510 MHz Analysis Bandwidth
- N9032B and N9042B:
- Hardware instrument software version A.45.03 or later
Option R10, R15, or R20
Supported gate trigger styles when segmented capture is enabled:
- ADC Mag (N9032B/N9042B)
- IF Mag (non-N9032B/N9042B)
The segmented capture feature will be disabled when the hardware does not support it or a signal path is selected that does not support it. When in Auto mode for the Signal Path, enabling segmented capture will constrain the measurement to only signal paths that support segmented capture which can result in the bandwidth and other parameters being limited because of selecting a signal path that supports segmented capture.
Helpful information for N9032B and N9042B users
At low gate trigger levels near the noise floor, segments may not be properly detected and will result in an error dialog rather than showing invalid data.
At shorter pulse repetition intervals (PRI) when using higher sample rates (span), the segments may not be properly detected and an error dialog may be shown instead of returning invalid data.
The signal may appear to jitter Variation in the amount of time that it takes packets to traverse the network and arrive at a destination. with respect to the first sample within a segment; however, the time of the signal relative to a signal in the first segment should be correct. The limitation is that the gate trigger ends up at some quantum boundary which can vary relative to the signal. Extra gate start delay, gate stop delay, or segment length (for fixed length segmented capture) may be needed as a result of this.
The maximum number of segments possible is not linear and varies as a function of sample rate, start gate delay, segment length, and stop gate delay. For fixed length segmented capture, the recording dialog can be used along with checking the Max Length checkbox to see a prediction of the maximum number of segments possible for the current setup. Since segments may vary in length when using variable length segmented capture, the maximum number of segments is not predictable for a given setup, although if something is known about the maximum or minimum length of the signal that may be captured in each segment, the fixed length segmented capture setup with similar gate delay and segment length may be used to help predict something close to an upper or lower bound (using the maximum and minimum length of the signal to be captured in a segment).
When using the trigger (arming trigger in the API 1) Access Preamble Indicator, or 2) Application Programming Interface) along with the gate trigger, the time shown from the trigger to the gate trigger may be inaccurate by a few hundred nanoseconds depending upon the system. It should, however, be fairly constant so that it can be measured with a known signal relative to the external trigger and compensated for on a given system.
ADC Magnitude is the only gate trigger style supported.
External Trigger is the only trigger (arming) style supported.
The ADCs used for segmented capture can have Sparkle Codes. If this occurs, incorrect gate triggers can occur for the segments in some situations. The Glitch Filter can be used to avoid triggering on these if this issue is encountered (see the Glitch Filter property in the Extended Settings dialog).
See Segmented Capture (Acquisition > Segmented Capture) for more details on using segmented capture.
Timestamp Source
Getting timestamps from X-Series Signal Analyzers is supported with the following requirements and conditions:
Firmware version A.37.01 or greater
IF Path supported timestamps: 140 MHz, 160 MHz, and 255 MHz IF Paths (option B1X, B1Y, or B2X) with X-Series Analyzers
Supported trigger styles
- Free-run
- External
- Periodic
- FMT
The Timestamp Source > Analyzer Instrument choice will be disabled when the hardware does not support it or an IF path or trigger style is selected that does not support it. See Timestamp Source (Acquisition > Segmented Capture) for more details on using timestamps.
Trigger (Arming Trigger) + Gate Trigger
Trigger (Arming Trigger) + Gate Trigger feature is supported by the same X-series hardware that supports Segmented Capture because the new arming trigger + gate trigger functionality requires the use of segmented capture.
The arming trigger is only supported when using an External Trigger Location of Trigger 1 or Trigger 2 (settable in the input extension parameters). The choice of external trigger for the arming trigger will not be shown until the External Trigger Location of 1 or 2 is chosen.
Only external trigger is supported as an arming trigger.
The Segment Capture Length Type additionally supports a value of Count & Timeout. Whichever is satisfied first (Count or Timeout) will cause the capture to end. Timeout is not precise, as it is a timeout and not a duration.
Triggering
The following trigger parameters are available for RF settings:
Parameter
Applies To
Frequency Mask
Frequency Mask
IF Mag (Video), External, External TTL, Periodic (see Slope and Hold-off Style Interactions), ADC Magnitude
Positive trigger delay is limited to 128 sec. Negative trigger delay is limited to the maximum length of the time capture or 128 sec, whichever is less.
Frequency Mask
Frequency Mask
IF Mag (Video), External, External TTL except in Free Run (see Slope and Holdoff Style Interactions)
Below Level or Above Level or conventional
IF Mag, External (External TTL is fixed at 2 V), ADC Magnitude
Frequency Mask
Periodic
Periodic
Frequency Mask
IF Mag (Video), External, External TTL, ADC Magnitude
Free Run, IF Mag (Video), External, External TTL, Periodic, Frequency Mask, ADC Magnitude
Periodic
Frequency Mask, IF Mag
Frequency Mask, IF Mag
Frequency Mask, IF Mag
Frequency Mask
The following trigger parameters are available for two-channel baseband (BBIQ) settings:
Parameter Type
Freerun
Channel
Channel Mag
External
External TTL
(See Slope and Hold-off Style Interactions)
The maximum length of the time capture for the MXA is limited to 4 MegaSamples at any sample rate (~21.4 Sec maximum).
N/A Seconds Seconds Seconds N/A N/A Conventional Below Level Conventional Conventional (See Slope and Hold-off Style Interactions)
N/A N/A Seconds N/A N/A N/A Volts Volts N/A N/A N/A Positive/Negative
Positive/Negative Positive/Negative Positive/Negative
Slope and Hold-off Style Interactions
When triggering on a positive slope with hold-off style set to Above Level, there is an additional interaction between trigger Hold-off and negative Trigger Delay. The sum of these two values is limited to the maximum capture depth, which is ~88 msec for spans greater than 10 MHz, and ~266 msec for spans 10 MHz and below. In addition, the trigger hold-off is limited to 80% of the maximum capture depth.
For example, at a measurement span above 10 MHz, where the maximum time capture length is 88.8 msec, the maximum trigger hold-off is limited to 80% of 88.8 msec, or ~71 msec. And, since the sum of the hold-off and the trigger delay must be less than the time capture length, the maximum negative trigger delay for a hold-off value of 71 msec would be ~17.8 msec.
Negative slope triggering + hold-off for external trigger is not supported by the 89600 VSA for X-Series Signal Analyzers.
Selecting the External Trigger Input Port
You can specify the external trigger input port (Trigger1 In or Trigger2 In) using the External Trigger Location hardware parameter.
Trig Out
Not all X-Series Analyzers models and options support the 89600 VSA Trig Out feature.
Refer to the Measurements book "Trig Out" topic's Unsupported Hardware table for more information.
See Also